Other Parts Discussed in Thread: MSP430F5329 HI All,
interfaced SDHC 4gb (class 4) card to msp430F5329 MCU.
My spi speed is less than 400Khzs.
1. getting response 0x01 from SD card after sending CMD0.
2. getting response 0x05 from SD card after sending…
Part Number: MSP430F5329
I am looking at 1.13.5.3 in SLAU208P it says
Vsense = TCsensor * Temp + Vsensor (eqn 8)
So solving for Temp
Temp = (Vsense - Vsensor) / TCsensor
so if
Vsense = ADC(raw)
Vsensor = CAL_ADC_T30 TCsensor = (CAL_ADC_T85 - CAL_ADC_T30…
Part Number: MSP430F5329 Other Parts Discussed in Thread: BQ40Z50 Hi,
I am curious about an issue I found when trying to communicate between two microcontrollers using I2C. I am using two MSP430F5329. Using the I2C on USCI B1 Base. The master only sends…
Part Number: MSP430F5329 Hi All,
I am trying to flash program through UART in to MSP430F5329.
getting Error is
MSP430: Can't Initialize Target CPU: **Error**: Serial Communication failed at port: COM9, baud rate:9600! To use serial monitor, please…
Part Number: MSP430F5329 I need simple code to read and write to I2C devices. The MSP430 is one master and the others are silicon devices. I find it amazing that you have so many variants of your peripherals that I can not find code that just works without…
Part Number: MSP430F5329 I have a system that has to be in a low power sleep mode that needs to wakeup every hour, take a temperature measurement, then go back to sleep. There are other modes that run full speed but I am not worried about them at this…
Part Number: MSP430F5329 In MSP430x5xx and MSP430x6xx Family User's Guide (SLAU208P) Paragraph 28.3.2 ADC12CTL1 Register
Bits 11-10 ADC12SHSx It says
00b = ADC12SC bit
01b = Timer source (see device-specific data sheet for exact timer and locations…
Part Number: MSP430F5329 I am running in standby mode which has the processor running at 10,000 Hz. I think the watchdog is turned off. I have replaced every instance that I can find of a watchdog reset, or watchdog init with a watchdog hold.
I have the…
Part Number: MSP430F5329 So 22118400 is a very convent number for a UART It also happens to be exactly 675 times 32768 Hz the frequency of REFO. When I try to use the UCS routines from the driverlib, I get 22085632 Hz which is exactly 32768 Hz away from…
Part Number: MSP430F5329 I am confused. the Datasheet MSP430F532x SLAS678D page 4 shows Pin 36 P3.0/UCB0SIMO/UCB0SDA
Pin 37 P3.1/UCB0SOMI/UCB0SLA So how do I configure P3.0 as a SDA and P3.1 as SLA
Here is what I tried.
void UCB0_Init(void) { // make this…