Part Number: MSP430G2433 Other Parts Discussed in Thread: CC3200 , MSP-FET , MSP-FLASHER Hi,
I'm trying to program the msp430G2433 with BSL from a host controller (CC3200) and have a few issue.
I have successfully implemented the BSL communication…
Part Number: MSP430G2433 Hi Champs,
I checked that datasheet which show Integrated effective load capacitance typical value in 5.22. However, it didn't show Min or Max. Customer would like to know does any drift offset on capacitor. Could anyone tell me…
Part Number: MSP430G2433 Other Parts Discussed in Thread: MSP430G2302 Dear MSP430 Champs,
Right now, we have a question on MSP430G2433 to implement Cap touch slider.
The question is on MSP430G2433, the cap touch sensitivity is too low and the cap touch…
Part Number: MSP430G2433 Hi ,
I have a capacity recharge circuit, what I want to do is get the voltage grow process of the capacity via AD converter, But I found that when the mcu working in 8MHZ mode, AD converter can touch the target value then return…
Part Number: MSP430G2433 Other Parts Discussed in Thread: SN65HVDA100 Question from customer:
To use the LIN function, do we need a LIN PHY in front of the MCU, or does it have one inside and we just need to use the UCARX pin? This is for the MSP430G2433IPW0RQ1…
Part Number: MSP430G2433 Hi Champs,
My customer found one piece MSP430G2433's content would be modified in aging test lab, and total volume in the lab is about 75 sets. The temperature is about 50℃, the moisture is about 75%. And the address is located…
Part Number: MSP430G2433 We have an issue with the MSP430G2433. When its Vcc voltage is slowly decreasing (it is driven by a 3.3V LDO which follows its input voltage, coming from a slowly discharging battery), if we get into deep discharge (i.e., the…
Part Number: MSP430G2433 I my application, one of the port is set as input I/O and monitoring signal which is either High (V = 3V) or low (V = 0.5 V). based on status of this input pin MCU makes very important decisions.
Which method between polling vs…
Hi Priyadharshini,
Our team is not familiar with the MCU programming of the RTC, I sorted out some old E2E posts that are regarding programming, hopefully they can give you some insight. If not, maybe you can make a post to the Microcontroller forum for…
Part Number: MSP430G2433 Hello,
I have a situation where MCU Vcc = 0 V and one of the I/o port which is set as input port has voltage higher than 1.5V, one of the MCU port (set as output) turns high and low.
Does anybody witness this and what could be…