Part Number: TPS6521905 Tool/software: Hello!
I want to design the 48V input power system.
So, I need the Power Management IC which have multi output voltages such as 5V or 3.3V etc...
I have searched TI PMIC products, but I can't find.
Is there…
Well it seems that installing the latest multi-cal system software download on another computer seems to have gotten me communicating with both UUT modules (these are PGA308 modules),
My HP33401A meter now reads a voltage which I am presuming is Vout…
Part Number: CC3100BOOST Other Parts Discussed in Thread: TM4C123GH6PM , CC3100 , CC3135 , CC3120 Hello TI community,
I began using TI TM4c123GH6PM development board for the first time after taking a course in edx on embedded systems. Under the topic multi…
Hi Fabiana,
Fabiana Jaimes said: This is a known issue where we see the CSI2RX SHIM DMA context channel 0 accepts all handled data. Due to the driver implementation, all of the other sensors are still streaming so when one (or a subset) of cameras in a…
Hi,
You don't need to add this into an Yocto build.
1. Please add your .service file into the following location: root@am62xx-evm:/etc/systemd/system# ls
basic.target.wants graphical.target…
Part Number: TDA4VM Other Parts Discussed in Thread: AM67A , SYSCONFIG Tool/software: Hi,
This is related to the following post:
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1376000/tda4vm-multi-camera-streaming-failed-and…
Hi Linto
No need to flash again these file
fatload mmc 1 ${loadaddr} Multi/u-boot.img //It is already present in the combined app image mmc write ${loadaddr} 0x2400 0x1000 fatload mmc 1 ${loadaddr} Multi/uEnv.txt mmc write ${loadaddr} 0x3400 0x100 fatload…
How to use a high side switch (HSS) to implement one fail all fail in a multi-module automotive LED rear light system?
A typical LED based rear lamp, shown in Figure 1, consists of several lamp functions such as tail, stop and turn signals. Based on the…
Here's a log from the device during boot:
DLPC7540EVM_UART_log.txt
----------------------------------------
Debug opened on URT0
I2C Port 1 initialized as Master port
I2C Port 2 initialized as Master port
I2C Port 0 initialized as Slave…
Next, I set the jumper to J67 and obtained the log.
---------------------------------------- Debug opened on URT0 I2C Port 1 initialized as Master port I2C Port 2 initialized as Master port I2C Port 0 initialized as Slave port eeprom: Content validated Cal…