Part Number: ATL431LI Other Parts Discussed in Thread: BQ32000 , , REF3333 Hi team,
I want to use ATL431LI to achieve a li battery in(3.7 to 4.2V) 3.3V out application, the load is BQ32000.
Does this circuit work? What is the min dropout voltage of this…
Part Number: INA240 Other Parts Discussed in Thread: REF3333 , TIDA-00909 , , INA282 Is it possible to simulate the effect of PWM duty cycle speed increasing output amplitude with full REF being added to the shunts current measurement? Transient analysis of…
Thanks, Chris!
Code is the compilation from examples, except I'm use timer32, not timer_a for sampling interrupt.
Buffer is ina159, ref is REF3333. MSP432 part is battery powered.
I am glad listen what this MCU have good ADC itself and I try make…
Other Parts Discussed in Thread: ADS1255 , PGA281 , REF3333 , ADS1282 , REF5025 , ADS1281 Hello,
we're trying to design an input front end for ADS1255 which can handle +/-10V signals (40V full-scale range).
We already have an idea, but is there any suggested…
Hello:
I have a MSP430F5659 powered by a TPS63031 3.3V Buck-Boost Regulator and I have concerns about the reference voltage on the ADCa12.
Is it better to source AVcc pin from a 3.3 Reference voltage generator (such as REF3333) rather than DVcc (Switching…
Hi Luis,
How frustrating! This whole time I
thought I was at fault. Looks like a copy and paste error.
First, not knowing how to attach a
file (E2E), and having moved on to another project, I would like to
describe the answers to…