Part Number: TDA4VH-Q1 Could you confirm if there are any internal hardware differences between the General purpose part (TDA4VH88TGAALYRQ1) and High security, R5F lockstep capable part (TDA4VH88T5AALYRQ1), or are these using the same silicon?
Part Number: TCAN1042-Q1 Hello team,
My customer mistakenly pull up the pin 5 in the Gerber, which should be NC, is there any influence? Is it necessary to change it?
BR,
Daniel
Part Number: TDA4AL-Q1 Hi TI Expert :
I have TDA4AL-Q1 MIPI CSI RX appliction question as blow list ,Pls help to clarify
Questions:
Does the TDA4AL CSI RX hardware support decoding up to 5 Data Types simultaneously in a single stream?
…
Part Number: LM706A0-Q1 Other Parts Discussed in Thread: LM706A0 Tool/software: Hi all,
I use LM706A0 EVM board to test 48Vin/3.3Vout@max 10A condition and see the transient regulation out of 5%.
Transient condition is 4A to 10A with 2.5A/us, using…
Part Number: TCAN1043A-Q1 Hi,
My customers now are considering using TCAN1043A-Q1 in a 5Mhz network with more than 5 nodes in this network. While, they still have concerns on the signal quality and also wondered if they should use CAN SiC device instead…
Part Number: TCAN2845-Q1 Tool/software: Hi,
One of my customer is considering TCAN28473/5 for automotive design. We are planning to use this regulator supply 3.3V to an off-board sensor, and it is essential that this supply is protected against both…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: TPS22919-Q1 Hi,
We'd like to use implement the signal connections as outlined in Figure 3-2 of the TPS65941319-Q1 User Guide ( www.ti.com/.../slvuci5a.pdf).
My understanding is that the GPIO3…
Part Number: DP83TG720S-Q1 Hello, We are looking for an integrated circuit that performs the conversion from automotive Ethernet (BASE‑T1) to an SLVS differential interface with the following characteristics:
Input interface :
Compatible with…