Part Number: SN65MLVD206 Tool/software: Hi Team,
Our customer would like to confirm if the SN65MLVD206 can convert a LVDS clock into single ended.
Regards,
Danilo
Part Number: SN65MLVD206
Hello,
In a harsh industrial environment I am having problems with a M-LVDS communication where the signals shared between transmitter and receiver are A,B and GND.
In AN-1926 states the following: "System designers building…
Part Number: SN65MLVD206 Hello support,
We would like assistant with one on your parts SN65MLVD206D/ Half-duplex M-LVDS transceiver . We need 2000 ASAP for one of our projects for BAE Systems EPAWSS. Rated D0-A1.
Please let us know where to find it…
Part Number: SN65MLVD206 Other Parts Discussed in Thread: SN65MLVD207 Hi Team,
My customer use SN65MLVD206/207 between CPU board and daughter board for communication:
they have 1 CPU board(1 sn65mlvd206), 1 mother board(2 100 ohm terminal resistor…
Part Number: SN65MLVD206 Hi Expert,
my customer is using SN65MLVD206, there is one question needing your help.
VIT+ in type 2 is 150mV for active positive-going differential threshold. if we meet a real signal in the input, which will have a drop…
Part Number: SN65MLVD206 Hi Team,
Good day!
Could you share the ESD ratings information of sn65mlvd206dr? I didn't find it in datasheet. Thank you in advance.
Best regards,
Jonathan
Part Number: SN65MLVD206 I needed to simulate a circuit that uses SN65MLVD206D. But I haven’t found any PSPICE or LTSpice model/part for it. PSPICE part will be preferable since I have already built the circuit in PSPICE with almost all other parts/components…
Part Number: SN65MLVD206 Hello Team,
My Customer is using the SN65MLVD206 for a SPI clock transmission/reception. RE & DE pins are wire-ored (shorted together) and connected to a GPIO of a uC. The uC controls the state of these pins by pulling high…
Part Number: SN65MLVD206 hi dear supporting team,
customer want to use one SN65MLVD206 driver to drive multiple SN65MLVD206 receiver, the clk rate is 8kHz, how many SN65MLVD206 is allowed as the loading? tks a lot!
Part Number: SN65MLVD206 Team,
I have a question from a customer per the below circuit configuration. Is it OK to short the two signals - RE+DE and R+D?
The two signals RE+DE and R+D are wire-ored. The R/D signal is being used for SPI clock connected…