Part Number: SN74AUP1T17 Other Parts Discussed in Thread: SN74AXC1T45 , SN74AXC8T245 Hi,
We would like to level translate 3.3V 125MHz LVCMOS clock signal to 2.5V level.
I have tried looking into logic device datasheets to identify suitable device to support…
Part Number: TLV3501 Other Parts Discussed in Thread: SN74AUP1T17 Dear Team,
Any advice for the comparator design about TLV3501?
Regarding the sqr2sine design, we found a lots of harmonics at 30/50/70/90Mhz when using square as output waveform, and it…
Yes, 2.5 V is high enough for LVC at 3.3 V. But the actual switching threshold is near V CC /2, so the propagation delays for rising and falling edges will not be symmetrical. (There are single-supply devices with lowered input switching thresholds like…
1.8 V is less than 1.92 V, so this is not guaranteed to work.
You have to use a device with lowered input thresholds like the SN74AUP1T17/SN74AUP1T50, or a level shifter like the 2N7001T, SN74AUP1T34, TXU0101, or SN74AXC1T45.
Other Parts Discussed in Thread: SN74AUP1T17
I am planning to use TI's LOW POWER, 1.8/2.5/3.3-V INPUT,
3.3-V CMOS OUTPUT, SINGLE SCHMITT-TRIGGER BUFFER GATE (PART NO: SN74AUP1T17) in
my design. I would like to know if this particular…
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74AUP1T17 Hi Experts,
My input signal with a low 17V/s slew rate for SN74LV1T34, does it will work normal?
Thanks!
Best Regards,
Xing
This device is not a level shifter and expect 3.3 V input signals. Devices with lowered input thresholds are the SN74AUP1T17 or SN74LV1T34. The fastest shifter is the SN74AXC1T45.
Part Number: 2N7001T Other Parts Discussed in Thread: TXS0102 , SN74AUP1T17 , SN74AHC1G125
Can I have a switching waveform as like this?
I want to confirm a good low noise signal transfer/receive device.