Part Number: SN74AXC4T245-Q1 Other Parts Discussed in Thread: TXB0104-Q1 What are the specific differences in usage between SN74AXC4T245-Q1 and TXB0104-Q1, and can they be replaced with each other?
Part Number: SN74AXC4T245-Q1 Dear Team,
We are using SN74AXC4T245QPWRQ1 part in our design, And we have connected one signal in wrong direction.
Because of this we are not seeing any issue for our use case and application.
Our concern is due to this…
Part Number: SN74AVC4T245-Q1 Other Parts Discussed in Thread: SN74AXC4T245-Q1 Hi team,
Could you provide a comparison between the SN74AVC4T245-Q1 and the SN74AXC4T245-Q1?
Are they able to use a 1kΩ pull-down resistor on the output side?
Thank…
Part Number: SN74AXC4T245 Other Parts Discussed in Thread: TXV0108-Q1 , TXV0106-Q1 Hi Team,
We are using the SN74AXC4T245PWR IC for level translation. In the datasheet, it is given that the data rate supported whea.n translating from 1.8V to 3.3V is up…
Part Number: SN74AXC4T245-Q1 Hello team,
We encountered some questions when evaluating the current consumption of two levelshift CAXC4T245QRSVRQ1 CAXC4T774QRSVRQ1.
In the Datasheet, the current consumption of ICCA and ICCB is at the uA level, but these…
Part Number: SN74AXC4T245-Q1 Hello team,
My customer want to double confirm whether DIR pin can connected to GND or VREF_A directly?
Do not need to add the res between DIR pin and GND/Power?
I think it is Okay for our IC, but it may need add some Res…
Part Number: SN74AXC4T245-Q1 Hello team,
Can I ask about the thermal pad of CAXC4T245QBQBRQ1 (WQFN) ? Are you recommending that it must be connected to GND or left open?
Thanks,
Sam Lee
Part Number: SN74AXC4T245 Hi, we are testing SN74AXC4T245 performance in the hope that we can use it as 3.3 to 1 V level translator. The pulse frequency operates at either 120 MHz or 60 MHz. We verified that at the input of the level translator, it is a…
Part Number: SN74AXC4T245
Could you tell me the operating frequency (max) for the following voltages ?
1.VCCA : +1.2 [V] / VCCB : +1.2 [V]
A port -> B port
B port -> A port
2.VCCA : +1.2 [V] / VCCB : +0.9 [V]
A port -> B port
B port …
Other Parts Discussed in Thread: SN74AXC4T245 Hi E2E,
I am planning to use SN74AXC4T245 as a 120 MHz clock 3.3V to 1V signal translator. Please advise if it is an ideal part. There are 8 synchronized clocks that needs to converted from 3.3V to 1V. If I…