Part Number: SN74CB3Q3245 Dear Team,
Here is Kevin from Delta Taiwan team.
Originally, customer was using TS2DDR2811 which had be EOL.
So we propose SN74CB3Q3245RGYR, but it is a low active device.
I check the portfolio, it seems we don't have high active…
Part Number: SN74CB3Q3245 Hi team,
Good day.
Is the junction temperature Tj of SN74CB3Q3245RGYR is the same as the storage temperature which is 150°C?
Thanks.
Regards,
Carlo
Part Number: SN74CB3Q3245 Hi,
do you have a switch/mux in BGA package?
The 6+ way, 3.3V tolerant analog switch/mux SN74CB3Q3245 fits nicely, but isn't available in BGA.
Do you have sth similar in BGA?
Thanks
Fred
Part Number: SN74CB3Q3245 Other Parts Discussed in Thread: SN74CB3Q3345 Hi Shashank,
is there a possibility, that there is a part, pin2pin, of course, that does everything that SN74B3Q3245 does, just invertet?
So this table
But when OE is low, nothing…
Part Number: SN74CB3Q3245 Other Parts Discussed in Thread: SN74CBTLV3245A Hello
When /OE is high,the device will consume how much current ?
what's different between Ioz and Icc ?
The four AD signals are bidirectional, and there is no direction control signal. It is not possible to buffer the LPC signals.
The SN74CB3Q3245 has an analog bandwidth of 500 MHz. What is the clock frequency?
Part Number: SN74CB3Q3245 Hi,
I would like to confirm that if VCC = 3.3V and if Ax is at 5V, does the Bx will be clamped at 3.3V or will reach 5V ?
Thanks.
Part Number: TLC555-Q1 Other Parts Discussed in Thread: SN74CB3Q3245
Hi Team,
The customer found that the IO model of SN74CB3Q3245 cannot be set as output, why? Could you pls help? The output high-level duration tH: 0.939 x 49.9k x 4.7uF = 162ms.Is this…