Other Parts Discussed in Thread: SN74AUP2G80 , SN74LV4040A , SN74HC688 , LMK00804B , SN74AUC74 , SN74LVC2T45 , CD74AC161 , SN74LV8154 , SN74HC4040 I need to make a 32 bit frequency counter for 150 MHz. Probably first part of counter would need to be ECL. parallel…
Other Parts Discussed in Thread: SN74LV8154 I need to measure the frequency of a signal, and feed the measured value to a small computer via an SPI or I2C interface for a remote sensor application. I could use two components for this (F-V converter & A…
Hi Apurv,
GPIO or NHET can be used to interface with SN74LV8154 IC. I don't know how to use SN74LV8154 device. Please check with experts in logic forum:
https://e2e.ti.com/support/logic/f/151
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74LV8154 ,
Hey, everyone!
I am using SN74HC165 shift register IC for reading parallel output data from a binary counter IC (SN74LV8154). How do I read the serial data output from this IC? Is it…
Part Number: LAUNCHXL2-RM57L Other Parts Discussed in Thread: SN74LV8154 , RM57L843 , HALCOGEN , DP83630 Hey, everyone!
I need to read 8-bit parallel data from SN74LV8154 binary counter IC using Hercules RM57Lx LaunchPad.
I want to use gioGetPort function for…
Hey, Michail, thanks for the reply!
The output characteristics of my module are the following:
maximum counts = 15,000,000 per second
pulse width = 35 nanoseconds
voltage = 0-3.3 V
dead time (minimum time between pulses) = 50 nanoseconds
I came acr…
Hi Mitch,
There are dual counters, like the SN74LV8154, but I don't know of any that count on both clock edges. The only solution I could think of would be to add a monostable multivibrator (pulse generator) to trigger on both rising and falling edges…
Other Parts Discussed in Thread: LMK03806 , LMX2581 , SN74LV8154 , LMK04828 1. Is there any method so that we can measure an activity with nanoseconds resolution?
2. I need to measure time taken by two bluetooth devices to send and receive 1 bit and distant…
Part Number: SN74LVCR162245 I would like to use the transceiver to control USB and HDMI signals. However I could not find the maximum supported data rate in the datasheet.
Would appreciate if the information can be provided.
Regards,
Ata