Other Parts Discussed in Thread: LMK00804B-Q1 , SN74LVC2G157 Hi,
Does anyone have any idea how much jitter is added by logic chips? I have a 16 MHz sample clock driving an ADC, but I want to have it MUXed so users can select an external synchronization…
Other Parts Discussed in Thread: SN74LVC2G157 , SN74CBTLV3257 , TS5A23157-Q1 , TS3A27518E-Q1 Hi Sirs, Would you please advise suggestions of automotive grade 2:1 MUX for I2S signals for 3.3V level of 12.288MHz MCLK, 3.072MHz BCLK, 48kHz LRCK, DIN and DOUT…
Gilad,
The main difference between SN74LVC1G3157 and SN74LVC2G157 is on is a passive FET switch with no drive capability and the other has drive capability.
You can see the SN74LVC2G157 has drive capability by the Voh and Vol specification while the…
Part Number: ADS1248 Other Parts Discussed in Thread: ADS1218 , SN74LVC2G157 , PCA9535 Hi,
I configured the ADS1248 to power down mode by taking the START pin to low.
VDD is connected to 3.0V and AVD is floating (The analog power was shut down).
According…
Hai Lenli,
I solved the problem using a 2:1Mux( www.ti.com/.../SN74LVC2G157) , its enough for me(Because I just need the tx line from GPS).
It is possible to emulate the second UART on the sensor conltroller engine(Only one per project).
Thus you can achive…
Other Parts Discussed in Thread: ADS1282 , ADS1256 , PCA9535 , OPA1632 , ADS1282EVM-PDK , SN74LVC2G157 Hi,
I have to interface ADS1282 with a microcontroller. I need to use SPI to do so. I went through the datasheet and its pretty confusing, I didn't get any…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…