Hello,
Very interesting what you're running into. I just did a quick sanity check on an EVM I have here with your exact register values you provided. It works as expected for me. The timer does reset the state machine after 3 seconds.
Let's try…
Other Parts Discussed in Thread: TCA8418 , TCA8418E-EVM Hi,
I had bought a TCA8418E-EVM board and I cannot driver TCA8418 successfully.
The cpu is C5515 and using custom board.
Please guide me about TCA8418 driver.
(1) Should I set TCA8418 config before…
Other Parts Discussed in Thread: TCA8418 , MSP430G2553 Hi there,
I'm trying to read from register once an interrupt is set by a button press on a keypad hooked up to a TCA8418 (EVM). I followed this setup guideline in the datasheet:
But only perform…
Other Parts Discussed in Thread: MSP430G2553 , TCA8418 Hi,
I'm trying to get a TCA8418 EVM/boosterpack to work with the MSP430G2553 launchpad from CCS. I'm using this TI guide to setup I2C:
http://www.ti.com/lit/an/slaa382a/slaa382a.pdf
But I'm…
Other Parts Discussed in Thread: TCA8418E , TCA8418E-EVM Dear All,
We are using TCA8418E with the AVR microcontroller in our application. For testing, a TI TCA8418E-EVM together with an ATMEL STK500 are being used at the moment.
The TCA8418E INT pin is…
Other Parts Discussed in Thread: TCA8424 , TCA8418 , TCA8418E , MSP430G2553 , TCA9546A , TCA9543A Hello team,
One of our customer wants to use several TCA8424 on the I2C bus, but the device has a unique I2C ID.
According to the datasheet of TCA8424 , " Other…
Other Parts Discussed in Thread: OMAPL138 , TCA8418 , TCA6416 Hello All,
I am following the below post to port TCA8418 to OMAPl138 EVM.
http://e2e.ti.com/support/interface/etc_interface/f/390/p/202938/757229.aspx#757229
I am able to successfully interface…
Dear Ahmad,
I have checked RTC_PORz when i reset the board.It is never toggled and always gives 1.8V even in power off condition also.
Out product does not have internet access. So i can not pull the time via NTP.
My dts file has following entries related…