Part Number: TCAN1042DEVM Other Parts Discussed in Thread: TMS320F28379D , TMS320F28388D For running the can_external_transmit on 28379d I am using two TCAN1042DEVM transceivers. The connections are as shown below:
I have configured the GPIOs properly…
Part Number: AM3358 Other Parts Discussed in Thread: TMDSSK3358 , TCAN1042DEVM , SYSCONFIG Tool/software: TI C/C++ Compiler Hi. TI.
I would like to add CAN function to TMDSSK3358.
I would like to use the TCAN1042DEVM product in the following configuration…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3507 , , TCAN1042DEVM Hi Ti,
Could we possibly use two EVB boards(MSPM0G3507), with one board as RX and the other as TX, for CAN bus communication testing?
I used the CAN-FD single RX and…
Part Number: TCAN1042DEVM hello,
Kindly assist me in configuring the TCAN1042evm for my project.
1. I wish to configure this module with VIo as input for VRXD.
2. Do I need to give a supply to VRXD (3.3V - 5V)
3. with the following configuration, I find…
Part Number: MSPM0G3507-Q1 Other Parts Discussed in Thread: TCAN1042DEVM , ISO1050 , SYSCONFIG Hi TI
I have used MCAN single message tx example from MSPM0 SDK . and in the case of TCAN1042DEVM I am using ISO1050 Isolated CAN Transceiver,
The problem is I…
Part Number: MSPM0G3507 Other Parts Discussed in Thread: TCAN1042DEVM Dear TI,
I am debugging following example code " mcan_message_rx_LP_MSPM0G3507_nortos_ticlang " to receive the data from my python script.
( python script is interface with ST…
Part Number: TCAN4420 Other Parts Discussed in Thread: TCAN1042DEVM , Team,
can TCAN1042DEVM be used for TCAN4420?
http://www.ti.com/tool/tcan1042devm
Thanks,
A.
Part Number: MSPM0G3507-Q1 Other Parts Discussed in Thread: MSPM0G3507 , TCAN1042DEVM
Hello TI Team,
I am facing a problem regarding CAN transmit signal detect on CRO.
I am using " mcan_multi_message_tx" example code from "mspm0_sdk_1_20_01_06" in MSPM0G3507…