Is there a datasheet for this actuator? It would be helpful to know what its electrical characteristics are.
The TX signals uses two inverter outputs in parallel. At 5 V, HC has a rated drive strength of 4 mA, so I assume the input needs 8 mA. A single…
Part Number: TCAN330 Tool/software: TI-RTOS Hi Sirs
Since I don't see rise time and fall time MAX/MIN in TCAN330 spec as below.
Could you help to share the value with me? Thank you a lot.
Part Number: SN65HVD230 Other Parts Discussed in Thread: TCAN337 , TCAN330 Dear TI experts,
My customer drew their schematic with SN65HVD230. Could you review the schematic?
And here are more questions ;
1. Is there any recommended schematic for OBD of…
Part Number: TCAN330 Other Parts Discussed in Thread: TMS320F28030 is there an open CAN stack for a Cortex-M3 MCU (Gecko) to drive the TCAN330? The MCU does not have a build in CAN interface.
Hi José,
José Arbugeri said: Firstly, I encountered an issue with this topology where one port of node loses connection with the network, causing the transceiver to become unterminated (60R). This situation leads to an unattenuated signal, and the…
DCAN1 is connected correctly....that schemo I posted is the "xceiver" board. verified connectivity from the TCAN330 to the Launch at J10-44,45...
TX at J10-45 is the data FROM hercules to the BUS (goes to the TCAN330 pin 1......RX at J10-44…
Part Number: TCAN337 Other Parts Discussed in Thread: TCAN330 , TCAN334 Hi experts,
Could the pin5 and pin8 of TCAN330/2/4/7 be tied to GND?
BR,
Gordon
Part Number: TCAN330G Other Parts Discussed in Thread: TCAN334 , TCAN330 Replace tcan334gdcnr with tcan330gdcnr. Without this function, 334G PIN8 is connected to GND.
Is tcan330gdcnr also connected to GND?
Hi Chris,
after some thinking I have decided to use SN65HVD232DR with controlled VCC, which will enable/disabled the IC completely. It seems like the most effective solution for me.
Since SHDN pin of TCAN330 needs to be pulled HIGH for low-power mode…
Part Number: TCAN330G Other Parts Discussed in Thread: TCAN330 HI,
we updated our hardware from ATA6561-GAQW-N to TCAN330 transceiver ATA6561 is working with +5V supply TCAN330 is working with +3.3V supply.
Now our CAN communication is not woring with the…