Part Number: TCAN334 Other Parts Discussed in Thread: TCAN1044A-Q1 , TCAN1042-Q1 Hi Team,
I want to find a can phy's TXRX withstand voltage could be 5V!
Because customer MCU is 5V! Does TCAN334 meet this need?
Or could you recommend another solution…
Hi Sean,
Thanks for the link and also the part recommendations.
We are doing a new board spin and I was considering changing to the newly discovered TCAN3413 due to its much larger bus fault voltage.
If I were to change to TCAN3413, is there a single package…
Part Number: TCAN334 Other Parts Discussed in Thread: STRIKE Hello !
I have selected the TCAN334 for my CAN bus application, and I am currently designing ESD protections for my circuit. I selected the TCAN334 for its integrated ESD protection, exceeding…
Part Number: TCAN334 Hi Team,
My customer wants to know what's the voltage level on CANH&CANL would be if it's under RL=open and in dominant mode condition?
Best regards,
Albert Lee.
Part Number: TCAN334 I would like to swap function of I/O pins on our product from the CANH and CANL lines of the TCAN334 to other purposes using a high speed analog switch (like the Vishay DG636E). Will this work? What problems might this cause to the…
Part Number: TCAN334 Hi Team,
When TCAN334 is for receiver, if there is glitch on VID and the glitch voltage is between 0.5V and 0.9V shown in picture below, will the Vo(RXD) keep the same without change?
If the glitch voltage is below 0.5V or above 0…
Part Number: TCAN334 Hello, We’re working with the TCAN334 device and we have a question about the wake detect process.
The datasheet for that part states that it utilizes the wake-up pattern from ISO11898-5:2007. Our understanding of that standard…
Part Number: TCAN334 Hello,
We have a question regarding the TCAN334 datasheet. It seems like there might be a datasheet error.
Table 4 shows that the device is in standby mode when STB pin is HIGH. However Figure 22 shows that the STB pin needs to go…
Part Number: TCAN334 1.What should the capacity of "CSPLIT" be when the termination method is "Split Termination"?
2.What is "integrated pull down"?
Is it necessary to pull down SHDN and STB externally?