Part Number: MSP430F67791A Other Parts Discussed in Thread: TIDA-00555 Hello,
I need your help. I am referring https://www.ti.com/lit/ug/tiduah1a/tiduah1a.pdf?ts=1619964188419&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FTIDA-00454
I see figure…
Hi David Schultz,
Thank you for your reply.
Currently, I am implementing the TI reference design TIDA-00454. However, I am unable to locate the details for Phase to Phase measurements in the reference document.
Is it possible to measure Phase to Phase…
HI Chirag,
Below is a link with a list of the existing current transmitter reference designs; there a few designs that may be of interest, or provide circuit blocks / design ideas.
[FAQ] Are there reference designs that can help me build a 4-20mA transmitter…
HI Shibin,
As Kai has mentioned, on the current transmitter application, the main issue with the Howland Current source configuration is that could be sensitive to capacitive/inductive load and will likely become unstable while driving a long cable. There…
HI Shiblin,
- The XTR111 is a current output transmitter. On the multiplexer circuit above, when selecting the RLOAD = 249Ω, the resulting output voltage will change with any additional load impedance or resistance applied at the output of MUX U38…
HI Joe,
Below are a few XTR300 and XTR305 reference designs that could be of interest.
XTR300: TIDA-00454 , TIPD155
XTR305: TIDA-01633
Thank you and Regards,
Luis
thank you bryan for your reply,
actually i have gone through the design of https://www.ti.com/tool/TIDA-00454 and link what you shared. Now i made connection like connecting my sct003 15A/1V current sensor to the phase line of light bulb which is 60W and…
To find reference designs leveraging the best in TI technology – from analog and power management to embedded processors, visit https://www.ti.com/reference-designs/index.html . All designs include a schematic, test data and design files.
I will…
Hi, thanks for your reprise,
I understand that it's better use a current sense amplifiers that has less bias current than the current I want o measure and both you have recommended has low bias current.
Aside of this, I don't understand when you…