Matsunami-san,
Please see the attached TLC393 block diagram that I have prepared for your customer.
Regards, Thomas
PA - Linear Applications Engineering
Hi Thomas,
from your answer it is quite clear that you have read the datasheets carefully. However, the datasheet of the TLC393 doesn't state anything about the used ESD protection of the input stage. So your answer is only guessing what the author…
Hello Thomas, Is the VICMR behavior specific to the TLC393? I know most comparators that I have used will operate correctly as long as *one* input is in the common mode range. Delay time may not be in spec, but it will work.
-Ken
Other Parts Discussed in Thread: TLC393 , LM339 1. I am using TLC393 op-amp as comparator with 15V supply.
2. Inverting terminal is connected with 1:1 voltage divider (10M each), by 3V voltage source.So that voltage at inverting terminal is 1.5V. …
Part Number: LMC7215 Other Parts Discussed in Thread: OPA177 , TLC393 Tool/software: Hello,
I recently came across an informative post on EDN discussing how to test operational amplifier characteristics. However, I've encountered difficulties when attempting…
Part Number: LM2903 Other Parts Discussed in Thread: TLC393 I'm trying to test the Electrical Characteristics of the LM2903 on page 10 of the product's datasheet. Some of the parameters I am trying to test (Input Offset Voltage, Large-Signal Differential…
Part Number: TPS22810 Other Parts Discussed in Thread: TLC393
Hi,
I'm using TPS22810 and TLC393 with a constant current source as the main parts of a supercapacitor charge circuit. The goal is to charge with low current, discharge through TPS22810…
Part Number: TLV3404 Other Parts Discussed in Thread: TLC393 , THS4524 , Hello,
We are looking for the maximum pulse voltage that can withstand the inputs of TLV3404, TLC393 and THS4524. The pulse width is from 10 to 500µs. Could you help us?
Thank…
Hello Nitish,
It should recover to normal operation, but it may take a few more microseconds - longer than the normal propagation delay.
Is this a DC voltage? Or an AC signal or pulse? Are there any transients on the supply or output?
There are…
Hello,
Thanks for your prompt reply. I use TI part number : UCC2895, UCC27324, TLC272, TLC393 . . .
These are waveforms :
Vmain_trafo = primary voltage waveform
Vsec_trafo I = secondary voltage waveform (measured direct to the secondary…