Part Number: TLV1851-Q1 Other Parts Discussed in Thread: TLV1851 , ATL431 , TL331B Hello, I have TLV1851 with 3v3 supply, IN- @ 2.5V using for PWM logic level translation from 5Vmax, 7Vmax, 10Vmax pwm signals. Output is high impedance, and actually the…
Part Number: TLV1851-Q1 Tool/software: I just want to confirm that the input leakage with 0V supply will be ~55nA when IN+/- are at a positive voltage. Essentially, same behavior as seen in the 1.8V supply plot (Figure 6-9) in the datasheet, but with…
Part Number: TLV1851 Other Parts Discussed in Thread: TLV1821 Dear poeple
I have a question related about the TLV1851. As shown in my picture I want to use it as a voltagemeter.
If the voltage is lower than the reference voltage the output needs to…
Part Number: TLV1851 Hi team, in the datasheet of TLV1851 I cannot find any information on the differential input resistance of the device. To be able to compare this parameter to other devices, could you share some information on this? Thanks, Jens
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: TLV1851 Just downloaded and installed PSpice for TI Ver. 23.1-2024-S001
Created a schematic using a TLV1851 from the TI library. No matter what I do I always have some red dots on the schematic…
Part Number: TLV7031 Other Parts Discussed in Thread: TLV1851 Tool/software:
VBAT=3V
refer to schematic, when TLV7031 output is static, current comsumption should < 1uA. But current comsumption is about 300uA @output=low; 500uA @output=high And this…
Part Number: TLV1805 Other Parts Discussed in Thread: TLV1851 , Tool/software: Hi Team,
As per the datasheet, IN+ and IN- are tolerant upto Vcc + 0.3V with Vcc (abs max) = 40V.
Now, I would like to understand the following, if Vcc=24V; can IN+ and…
Part Number: LM7341 Other Parts Discussed in Thread: TLV1811 , TLV1841 , TLV1851 Tool/software: Will the input bias current increase when the LM7341 is used as comparator? The differential voltage between the inputs is 1-4V and well within the supply…
Part Number: TLV1811-Q1 Other Parts Discussed in Thread: TLV3701 , TLV1811 , TLV1851 I was using the TLV370X series parts these parts are no longer recommended for new designs. Looking at parts, I feel the TLV1811 would be a more appropriate replacement…
Part Number: TLV1861 Other Parts Discussed in Thread: TLV1851 Tool/software: Designing a comparator using the TLV1861 to "shutdown" a solar charging component when the voltage on the photovoltaic panel falls below a level that will provide sufficient…