Hamid
Thanks for following up. The TLV3604 inputs are bound by VCC and VEE, so there is nothing that would clamp the input at -0.6V as long as the VEE is at -2.5V. If you are seeing the input clamp at approximately a diode below ground, that would indicate…
Part Number: TLV3601EVM Other Parts Discussed in Thread: TLV3601 , TDC7201 We are using TLV3601/03 EVM for ToF measurement.
Detector output signal connected to Non inverting terminal and a ref voltage at inverting terminal of TLV3601.The out of TLV3601 is…
Hi Deepak,
As Clemens mentioned, we have seen TLV3601 be used to convert differential outputs to single ended outputs but unfortunately this adds a delay being that TLV3601 is in the 2.5ns range and minimum pulse width of 1.25ns. Sorry this is the best…
Hi Anh,
Per the article that Jiyah posted, we recommend using a high-speed comparator for ToF systems if distance is your only concern.
Our portfolio has several comparators with low dispersion and narrow pulse width detection. For an LVDS output option…
Part Number: TLV3603 Other Parts Discussed in Thread: TLV3601 I tired to simulate the model in my own design, as well as in reference design provided with model. In both cases it is not working. I used TLV3601 before and it worked, so maybe there is error…
Part Number: TDC7201 Other Parts Discussed in Thread: TLV3601 , Hi,
Customer question:
Is impedance matching required between the output of the comparator (TLV3601) and the input STOP2 pin of TDC7201?
Thanks,
Tyler
Jimmy,
We have many devices in high speed niche. Can you share any details in your system and comparator requirements besides 5V?
For 5V, we have TLV3201 (40ns) and TLV3501 (4.5ns), TLV3601/2/3 (2.5ns), TLV3604/5 (800ps, LVDS) and TLV3801/11 (225 ps,…
Part Number: TLV3601EVM Other Parts Discussed in Thread: TLV3601 Good morning,
I am going to purchase a TLV3601/3603 evaluation module, and want to clarify if the EVM comes populated with all components. Most of the images appear to show an unpopulated…
Other Parts Discussed in Thread: SN74AUC1GU04 , TLV3601 We have a laser trigger pulse which has 250mV amplitude and 2 ns pulse width. We would like to seek a simple solution to shape the laser pulse to 3.3 LVCMOS level and at least 30ns pulse width. Any…