Part Number: TMS320VC5402 Other Parts Discussed in Thread: TMS320VC5502 I want to find the download website of file ".brd" about TI DSP TMS320VC5402 for JTAG debugging and programming.
I want to find the user manual (user guide) about JTAG daisy…
Other Parts Discussed in Thread: USB2ANY , TMS320VC5402 Hello,
I'm just getting started with an evaluation board that interfaces to a computer through a 25 pin IEEE printer connector. I don't have any computers with that kind of port built in; my laptop…
Part Number: TMS320VC5402
Hello everyone,
My issue is related to the reset conditions of the DSP C54x.
So, I did my reset design bu using a simple RC circuit. refer to picture below.
1/ Sometimes, I'm getting an issue with DSP hangs (not running FW)…
Part Number: TMS320VC5402 Tool/software: Code Composer Studio 1、The /NMI and /BIO pins are all pulled up through the 10K ohm to the 3.3V;
2、All CVDD pins voltages are normal to 1.8V,All DVDD pins voltages are normal to 3.3V,All the VSS pins are normally…
Part Number: TMS320VC5402 Tool/software: Code Composer Studio Originally posted in error for different DSP
I am trying to clarify behaviour in casting from float to a short integer in the event that output data exceeds +/-32767.
I can see compiler is…
Part Number: TMS320VC5402 Hi,
My issue is related to the drift of DSP C5402 timer.
details:
- I'm using a TCXO as an external source clock X2/CLKIN: link here.
- View the accuracy/stability of my TCXO 0.5ppm, the drift should be within 2ms/hour.
…
Other Parts Discussed in Thread: TMS320VC5402 Hi,
I have done a program about the TMS320vc5402, and it's can do well by CCS2.2. Because I want run it in CCS3.3, I must transplant the program.
I used the CPU is TMS320vc5402, and the CPU connect with…
hi there
I’m working on the project with TI DSP 5402, I wrote the mix code including assembly and “C” , which is running fine with emulator, but it could fail to one function when it come to machine running ( after crossload), do you have any experiences…
Other Parts Discussed in Thread: TMS320VC5402 Hi, I’m beginning to work on TMS320VC5402 DSK, so I have some difficulties in the installation of the board (connected to the parallel port of the PC) and I need some help about:
- CCS studio installation…