Part Number: TLV320AIC3254EVM-K Other Parts Discussed in Thread: TLV320AIC3204 , TPA2012D2EVM , TLV320AIC3254 Tool/software: Hi,
I have a TLV320AIC3204_54_RHB_EVM board and the codec is TLV320AIC3254. I also have a TPA2012D2EVM and a 8 ohm/1.5w two…
Part Number: TPA3139D2EVM Other Parts Discussed in Thread: TLV320AIC3254 , TPA2012D2EVM Tool/software: Hi, I am an intern from a sports-related company, and I have been given a task to use TPA3139D2EVM and connect to a speaker to play sound from a computer…
Hi Sajid,
Can you try testing the amplifier separately by using the amplifier without the codec and supplying the input signal INL+/- with a waveform generator?
I tested your configuration on the TPA2012D2EVM with just the left channel input supplied…
Part Number: TLV320AIC3204EVM-K Other Parts Discussed in Thread: TLV320AIC3204 , TPA2012D2EVM , TPA2012D2 , LM48511 , TPA2011D1
Dear TI Technical Support Team,
Recently i have purchased the TLV320AIC3204 EVM kit to interface with my audio devices…
Hanazawa-san,
I have tried with TPA2012D2EVM. Current consumption is lower after short at the output, similar to having the amplifier in shutdown mode. Device current consumption is normal after cycling SHUTDOWN pin to take the device back to active…
Hi Oswald,
The EVM is the TPA2012D2EVM . You can find it in the "Hardware Development" tab on the TPA2012 product page. The EVM has documentation for its layout and schematics.
Best regards, Jeff McPherson
Hi Sal,
I used the TPA2012D2EVM to perform the test. I configured the EVM based in the User's guide under the following conditions: Vdd=5V, Gain= 16V/V, differential inputs, RL=8Ω in each output and Vin=0.5Vrms. I mentioned to you the behavior previously…
Hi Beki,
What MEMS mic are you thinking of using? MEMS microphones can behave like traditional electret analog microphones with an integrated DAC to output a small amplitude signal. Or they can be a digital microphone - outputting a PDM stream of 1…
Hi V Pot,
Actually, the AIC3206 onthe C5545 BoosterPack has a built in charge pump specifically for the headphone output. This allows the headphone jack to output a slightly higher 5.8-mW without the large DC blocking caps and with the same 1.8V supply…