Part Number: TPL5100 Other Parts Discussed in Thread: MSP430F5529 hi,
I need 24 hour max interval timer for a low power IoT device and nanoamp current consumption.
Please suggest me part number.
Other Parts Discussed in Thread: TPL5100 I wanted to know whether the TPL5100 from the site: www.ti.com/.../tpl5100.pdf has the fuctionality of replacing a 555 timer chip and doing its job in a monostable circuit like the Youtube video from www.youtube…
Other Parts Discussed in Thread: TPL5100 Hi,
I am thinking of using the TPL5100 for one of the connectivity application, "Section 9: Power supply recommendations " recommend to power the device from 2.7 to 5.5V and in the features and in section "6.3 Recommended…
I want to wake up my µC with the TPL5100 every 512 Seconds.
For this i like to connect only the MOS_DRV pin to the Interrupt Pin on the µC (i have only one pin left).
So i can't send a DONE to the TPL5100.
Is this possible?
Hi Rodrigo,
since the TPL5100 has a MOS driver functionlaity, it is supposed that if the micro is power gated by the TPL5100 there is no way that it can send a done if the MOS_DRV signal is high.
When the MOS_DRV signal is high the TPL5100 doesn't expect…
Other Parts Discussed in Thread: TPL5100 is there a timer that gives higher interval(16 sec) tpl5100 ? I do not mind the power range.. but I cannot afford to program the timer. I would want it to be programmed via resistors.
answers much appreciated! …
Part Number: BQ25570 Other Parts Discussed in Thread: BQ25505 , TPL5100 Hello Ti,
We have a use case where our chosen solar panel outputs 2.25V @ 0.003mA in an environment where the indoor lighting is used (Normal Tubelights). This is a very critical application…
Other Parts Discussed in Thread: TPL5010 , TPL5110 , TPL5100 hello! I am asking for TPL5100, TPL5010 and TPL5110 LT spice model because i don't find it. If there isn't spice model for these reference, can you suggest me other similar timers for LT spice…