Other Parts Discussed in Thread: TS5A22366 Hi Team,
My customer is considering FMEA( failure mode effect analysis) of TS5A22366.
Could you tell me the switch function if IN1 and IN2 are open(High-Impedance)?
I think these are CMOS input and the function of…
Other Parts Discussed in Thread: TS5A22362 , TS5A22364 , TS5A22366 Hello,
I'm looking for an audio switch. They have only found the Pericom PI3A288 to meet all their requirements, which are:
1. Works at 1.8V and 3.3V
2. Chip-scale package
3. Negative…
Other Parts Discussed in Thread: TS5A22366 , SN74CBT3257C , TS3USB3000 , TS5A23159 Does TS5A22366 have specs about its input/output leakage when V+ = 0(GND)? like Ioff in the sn74cbt3257c datasheet.
Best regards, Zhaomin Lai
Part Number: TS5A23160 Other Parts Discussed in Thread: TS5A22362 , TS5A22366 , TS5A22364 Hi,
The TS5A23160 datasheet states the analog input signal range as 0-V+. I plan to input a signal in the range -25mV to + 25mV which means a slightly negative going…
Hi Shu-Cheng,
We do have parts that can compete with the FSA4480. You have found some competing parts looking at the TS5A22362, TS5A22364, and TS5A22366.
The main difference between the three are:
TS5A22362 audio signal switching
TS5A22364 audio signal…
Helen,
There is also a device family TS5A22362, TS5A22364, TS5A22366 that are designed for audio applications and can support negative voltage signals.
Thank you,
Adam
Other Parts Discussed in Thread: TS5A22362 , TS5A22364 , TS5A22366 , TMUX1574 , TS5A22364-Q1 , TS5A23157-Q1 Hi Sir,
could you please help to suggest a solution which support TDM 1:2/2:1 audio switch purpose?
Thanks
Other Parts Discussed in Thread: TS5A22366 , TINA-TI , TLV7011 Dear Team,
I am designing a circuit which will modulate 2.8V DC signal w.r.t to a data signal.This is accomplished by an opamp (non inverting configuration) and a transistoe as switch.
My I/P…
Jimmy,
There is more crosstalk data at the bottom of the TS5A3157 which shows this device has quite good performance at low frequency.
How are you observing the cross talk? Do you have a scope capture?
What type of audio are you signal are you using…
Part Number: TS5A22362 Other Parts Discussed in Thread: TS5A22366 e2e,
I have another question related to the TS5A22362 I was hoping you could help with.
The input logic high (min) is 1.4V for both 2.7 and 3.3V operation of the TS5A22362, but I wonder…