Hi Dongbao,
Dongbao Zhou said: e2e.ti.com/.../quote]
This thread is correct, and I believe it is valid for the TUSB216/I.
It is noted in the TUSB217A datasheet that the TUSB216 only has CDP functionality, meaning the BC1.2 Controller should only be enabled…
Part Number: TUSB216I Other Parts Discussed in Thread: TUSB216 , TUSB217A Hi team,
Customer is evaluating using TUSB216 in their project. They would like to support 2m pre-post cable and 5m post-channel cable.
In datasheet, we see there are test shows TUSB216…
Hi Josh,
What are the major differences between TUSB216I and TUSB217A? I can't see any obvious difference in terms of function and performance from the datasheet (other than TUSB216i has wider temperature range). However, we received a quote for both…
Hi,
Below is the suggestion from the team:
Since you are using a redriver here for signal conditioning, we suggest you don't connect the USB_P/N on TPS65987D and connect the USB_P/N to TUSB217A.
Regards.
Hi Novel,
1. TUSB211 does not come with any form of DC Boost, which means it will not really improve any levels of VHigh or VLow in an eye diagram, you will only see improvement in the rising and falling edges. However, every iteration after the TUSB211…
Part Number: TUSB211 Other Parts Discussed in Thread: TUSB217A , TUSB216I , TUSB212 Hi Team,
With reference to the below E2E thread, wanted to understand if the Table attached in the thread regarding Boost settings is applicable for TUSB211 as well?
Also…
Hi Kura-San,
TUSB213-Q1 and TUSB217-Q1 can be and have been used in these applications. I recommend TUSB216-Q1 and TUSB217A-Q1 as they are improved versions of TUSB213-Q1/TUSB217-Q1. TUSB216-Q1 and TUSB217A-Q1 both support Android Auto and Carplay.
1) All…
Hello Statham,
The TUSB215 is in a different package than the TUSB216 and performance is different.
Possible pin compatible devices are TUSB216I, TUSB217A or TUSB212. Please note that there are differences in device behavior between the versions:
https…
Hi Andy,
You can find a comparison table in the TUSB217A datasheet, see link below. TUSB216I BOOST pin configures both AC and DC gain. Level 1/2 works for most applications.
https://www.ti.com/lit/ds/symlink/tusb217a.pdf#page=3
Hi Koki-san,
1. TJ should not be 125C for either commercial or industrial variations. TJ limit for commercial part numbers is 85C and 105C for industrial part numbers. Are you referring to TUSB214-Q1 and TUSB217A-Q1?
2. There is not difference in the package…