Part Number: UCC2813-0 Other Parts Discussed in Thread: TL431 Hello,
We are trying to use the UCC2813-0 Switching Controller and we having problems getting it to function properly. Is there any applications engineer that we can work with?
Regards…
Part Number: UCC2813-0 Other Parts Discussed in Thread: UCC2800 Hi, here is the gate pulse plot for UCC2813-0 flyback controller.
I am trying to simulate this FBC operated in DCM in simetrix. The pulse width is not becoming constant even after reaching…
Part Number: UCC2813-0-Q1 Hello Guys,
Good day.
Kindly help to confirm if this device can be used to design an ac to dc converter with 24VAC to 265VAC input and 12VDC output. Customer need to make SMPS with this.
Thanks!
Art
Part Number: UCC2813-0 When determining the frequency using "UCC2813PWTR-0", there is a statement in the RC section of the delivery specifications to use the calculation formula below, but I do not know how much variation will occur from this calculation…
Part Number: UCC2813-0 Flyback Circuit - 02.21.24.pdf
I am having problems with what I think is overcurrent on the the IC that causes it to break down after some amount of time. I have broken the trace on my board and added a wire to measure the current…
Part Number: UCC2813-0-Q1 Other Parts Discussed in Thread: UCC28C40-Q1 , , UCC28951-Q1 Dears,
I'm looking for the best solutions of automotive application's high power boost converter. But It is not easy to find that solutions. Could you recommend it…
Part Number: UCC2813-5-Q1 Tool/software: Hi Team
It is weird that customer found the device UCC2813QDR-5Q1's RC pin will start to discharge when the Vrc reach to 1.7V but not 2.65V sometimes.
I noticed the DS claimed that UCC2813-X increased 2.65V…
Part Number: UCC2813-0-Q1 Other Parts Discussed in Thread: UCC28C42 Hi,
Is there any way to increase the soft start time to limit the inrush current? According to the d/s, the soft time maximum is 10ms but it's not enough.
Thanks
Dongbao