Part Number: TPS1H100-Q1 Tool/software: Hi Team,
May you help check if we can use 2*TPS1H100-Q1 as OR architecture. In addition, we will not let two TPS1H100-Q1 turn on at the same time.
I just want to check if there is any issue when body diode turn…
Part Number: SN74HC244-Q1 Tool/software: Hi,
Can you please clarify the difference between these 2 parts,
SN74HC244QDWR G4 Q1
SN74HC244QDWRQ1
Ver Urgent request. please clarify as soon as possible.
Thank you.
Part Number: CC2642R-Q1 Tool/software: My customer found that their central device(NXP KW45) still sends CONNECT_IND with CSA#2 when CSA#2 is already disabled on peripheral side(CC2642).
In BLE core spec 5.3, there are two sections which look contradictory…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27624 , UCC27531 Tool/software: I am planning to use the UCC27531-Q1 2.5-A and 5-A, 35V MAX VDD FET and IGBT Single-Gate Driver to drive the SCT2H12NZ 1700V, 3.7A, THD, Silicon-Carbide (SiC…
Part Number: LM74502-Q1 Other Parts Discussed in Thread: LM74502 , LM74721-Q1 Tool/software: Hi Team,
We are using LM74502 to drive a B2B MOSFET for reverse protection. Is the TVS necessary for the ISO7637-2 Pulse1 test? We need to pass the pulse 1 but…
Hi Wilson,
Thanks for your patience. I am still testing as I ran into some linker issues with vision apps. I will get back to you tomorrow regarding this issue. Thanks,
Neehar
Part Number: DS90UB954-Q1 Tool/software: We are experiencing the same issue as described in:
https://e2e.ti.com/support/interface-group/interface/f/interface-forum/720925/ds90ub954-q1-ds90ub954-q1-csi-2-output-has-good-data-but-no-clock
Unfortunately…
Part Number: TCAN1145-Q1
Tool/software:
1. Power on with VBAT = 13.5V.
2. Decrease the VBAT voltage to 4.2V.
3. Read the register value of MODE_SEL via SPI read command.
Then, the result is MODE_SEL = 001b (Sleep), but INH is still High.
(MODE_CTRL Register…
Part Number: TCAN1462-Q1 Tool/software: Hi team,
Could share which parameters are mentioned in ISO 11898-2:2016, Table14? Which parameters shown in TCAN1462-Q1 datasheet are corresponding to that?
Regards, Ochi
Part Number: AM625
Tool/software:
Hi TI Experts,
I have the below queries regarding the CSI-2 interface
Supported data rate
Does the CSI-2 interface provide provision for internal termination
Links to useful threads
Let me know your thoughts.