Part Number: DCA1000EVM
Hi E2E,
I just downloaded mmWave 2.1.1.0 and I have this error when opening it. I made sure to download MATLAB runtime R2015aSP1 (8.5.1) and the XDS Emulation Software.
...
[03:53:35] Matlab Runtime Engine is installed [03:53:35] [RadarAPI…
Part Number: DP83869HM Other Parts Discussed in Thread: USB-2-MDIO Hi there
I use a DP83869HM connected to a AM64 over RGMII and want to make compliance tests. I've cut the MDIO lines open and connected a MSP430 Launchpad to the PHY as described in SNLA239B…
Other Parts Discussed in Thread: TUSB1310 Hi.
We are looking for transceiver which supports for both USB 3.1 Gen 1 and USB 2 for the Combo Hub application with the PIPE as 32-bit SDR,
Could you please suggest regarding the mentioned for this.
Thanks, Joshua…
Part Number: MSP430F5328 Other Parts Discussed in Thread: USB-2-MDIO , DP83TG720EVM-MC Hi,
A customer of mine built his own board with DP83TG720S and he wants to use a MSP430 to program the PHY via MDIO. So the same approach as on the DP83TG720EVM-MC. Is…
Part Number: BQ25703A Hello, I was reading the datesheet of BQ25793A . I am looking for implementation of this IC to charge a 2-S lipo battery
But my doubt is if I could use this IC without MCU, I mean I would like to use only the BQ2579A with an USB-C…
Part Number: DP83TC814S-Q1 Other Parts Discussed in Thread: USB-2-MDIO I'm using the USB-2-MDIO application to investigate link behavior of a DP83TC81S-Q1. When I connect to my board, I see PHY0 through PHY15 listed as available. The behavior I was…
Part Number: DP83TD510E-EVM Other Parts Discussed in Thread: USB-2-MDIO I'm trying to power DP83TD510 and connected DP83822 with USB from PC or USB charger. I installed J9 jumper (USB power), and left all other jumpers as default (EXT pins left disconnected…
Part Number: USB-2-MDIO Hi,
I have connected the MSP430F5 to a DP83TC812 MDIO interface, using the USB-2-MDIO application, and I have seen that the response from reading a register is rotated.
See below: instead of default value 2100, the value is 4201…
Dharrvin
You can use either 100nF or 220nF for SSTX1 and SSTX2.
Does the FLIP pin change its voltage for the normal and flip Type-C orientation? You should see 0V on FLIP pin for the normal orientation and 3.3V for the flip orientation.
For USB3.2 Gen2…