Part Number: ESD401 Hi team,
Can our ESD401 be use to protect CAN interface? Or do you have any better recommend ESD device for CAN?
Thank you!
Yunjing
Part Number: ESD401 Hello
can we use ESD401 protection diode on 5V power line that will carry not more than 50mA current.
Or please suggest 5V power line ESD and Surge protection with smallest possible size.
Regards,
Raghu
Part Number: ESD401 Other Parts Discussed in Thread: TPD1E04U04 Dear Sir
I'm not expert in ESD protection line, I need to protect the I/O line, analog input, usb line and keypad line
on my items and I would like what do you suggest me in order to…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Part Number: TPD4E02B04 Other Parts Discussed in Thread: TPD1E01B04 , , ESD401 , TPD4E1B06 , BOOST-PSEMTHR-007 , ESDS304
Hi All,
I'm looking for a ESD and Surge protection (on data lanes) recommendation for 10Gbps PoE PSE Injector ( there is no ETH phy…
Part Number: TIDA-01411 Other Parts Discussed in Thread: TPD4E02B04 , TPD1E01B04 , ESD401 , TPD4E1B06 , BOOST-PSEMTHR-007
Dear *,
we are designing 10Gbps PoE PSE Injector, so we have a RJ45 data in connector and we want to protect this port.
Q1)
Would you…
Part Number: TPD1E01B04-Q1 Other Parts Discussed in Thread: ESD401 , TPD1E10B06 ,
Hi Erika,
Could you help to recommend the ESD diode for the UB933 and UB954? What’s the maximum IO cap for the FPD-link for these two parts?
Customer want to know what…
Hi Marco,
Unfortunately, we do not have any p2p part in that specific 3-pin package. For a non-p2p 2 channel solution, the best part would TPD2E009. However, if you want to go with 2 single channel devices, I would go with ESD401 or TPD1E05U06, like…
Other Parts Discussed in Thread: ESD401 Hello,
I have protected the input ports of the TLC272CDR with 2 BAV99 according first circuit drawing. Original the design was according the second circuit drawing and was sensitive for ESD. Due to the very low…
Part Number: TPD1E01B04 Other Parts Discussed in Thread: TPD1E6B06 , ESD401 We are currently using PESD5V0H1BSF
Can you please suggest part similar to TPD1E01B04DPLR with 5V Working Voltage in 0201 package dimensions