Part Number: DIP-ADAPTER-EVM We are planning to use your evaluation board to validate a new fabrication process.
Is it possible to get access to the Gerber for the pastemask top layer?
We could work with any part of the layout file that shows the top…
Part Number: SMALL-AMP-DIP-EVM Hi
Can you please provide the CE/EU Declaration of Conformity for SMALL-AMP-DIP-EVM?
This product appears to bear the CE-Marking but the EU D eclaration of Conformity is not available on the website.
Thank you
Hi Keerthi,
1.Could you please check with the dip switch settings that you have shared since SW7 and SW11 are push button switces.
And SW8 and SW9 are the boot switches for J721S2 EVM board correct? If yes, please share me the related dip switch settings…
Part Number: TPS62410Q1-EVM Other Parts Discussed in Thread: TPS62810-Q1 hi, I got a problem during the test of the demo board of the TPS62410Q1-EVM. When the power was turned on, I set two DC / DC outputs to 500mA at the same time (one connected to a…
Hi
Arjav Parikh said: SW11[1-8] = 1000 0010 SW7[1-8] = 0000 0000
This DIP switch configuration is for the SD card.Please check if your SD card already has images or not.If yes connect the UART cable to the Main UART as marked in below picture(2).
open…
Part Number: DIP-ADAPTER-EVM Hello Team,
it may sound trivial but can you share the schematics or layout, please? How are e.g. the SOT23-5 pins connected to the DIP-8 pins? 1->1, 2->2, 3->3, 4->4, 5->5 or 1->1, 2->2, 3->3, 4->6, 5->8?…
Part Number: OPA1679 Other Parts Discussed in Thread: OPAMPEVM-PDIP Hi team
Is there any evaluation board which customer can evaluate easily? I only found DIP conversion board
QFN16-DIP-EVM
Best regards,
Hayashi