Part Number: BQ25750 Other Parts Discussed in Thread: BQSTUDIO
Hello,
Here is a link to the BQ25750 BQZ file: Charger_1_00-bq25750.bqz
To install this bqz file, download the file and move it to the config folder of the BQStudio installation. Best Regards…
Part Number: LMH1297
When signal goes through two different transmission line, signal may get reflected based on difference between these two medias impedances. Return loss is the ratio of the reflected signal to the launched signal. If signal goes through…
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62B ,
Overview
In some applications it is critical that SPI transfers happen with the smallest-possible inter-byte gaps to either optimize throughout, or to meet certain overall system real-time…
Part Number: TUSB522P Other Parts Discussed in Thread: TUSB1002A , TUSB1044 , TUSB542 Hi Experts,
I see parts like the TUSB1002A and 1044 described as "linear" re-drivers while the TUSB522P is a "limited" re-driver. Which one is better to use in a USB system…
Part Number: TUSB1002A Other Parts Discussed in Thread: TUSB1064 , TUSB1044
Hi Experts,
Will the TUSB1002A recover the loss before or after the re-driver?
Best,
Shane
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62 , , SK-AM62B
Overview
It is a common need wanting to incorporate a custom Linux device tree file into the boot process of Yocto-generated filesystem images. This FAQ introduces a simple and basic…
Part Number: AM2634
Hi experts,
I am using the out-of-box MCAL Eth app demo
How do I disable interrupt pacing in my MCAL Ethernet project
How do I switch to polling mode instead of interrupt mode.
Part Number: TPS2592AA Other Parts Discussed in Thread: TPS25924 Why is TPS2592AA status changed to NRND (not recommended for new designs) and what is the replacement for it.