Hi Kygo,
Thank you for the query on UCC28180.
I will provide my comment only for the UCC28180portion of the schematic.
Please find the schematic with comments and calculator tool for reference.
4774.sluc506c.xls
CHARGERD3_review.pdf
Regards…
Ben,
We do not use google docs for my group. Here are the instructions:
1. Click "Insert"
2. Click "Image/video/file"
3. Click "Upload"
4. Click "Ok"
0407.bq24610.pdf
I have uploaded the datasheet as an example.
Regards,
Mike Emanue…
Hi
Vicente
As shown in the attached file, LMX2594PSEVM is equipped with two PLL-ICs. Therefore, I think I can output 5.8GHz from one IC and 5.9GHz from the other IC. I would like to know this method. Do you have any good materials? LMX2594PSEVM.p…
Part Number: TPD3S714-Q1 Hi,
I received the question from my customer.
Does the TPD3S714-Q1 have the result passing the surge test of ISO7637-2?
The test is p.15~16 of the attached file(section 5.6.3 (Test pulses 3a and 3b)).
3438.ISO 7637-2-2011…
Hi Tiger,
I have attached a UB941AS datasheet with the package dimensions. I'll look into why the package dimensions aren't available on TI.com.
Best,
Jack
ds90ub941as-q1.pdf
Hi Reza
The DCLK_RST feature will function with an asynchronous input, but because setup and hold is not guaranteed there will be +/- 1 ADC clock uncertainty for the capture of DCLK_RST into each ADC.
To ensure all ADCs capture DCLK_RST on the same…
YiKai Chen said: As I know, there is no limitation on these items.
Hi YiKai, thanks for your reply!
However reading STANDARD TERMS AND CONDITIONS FOR EVALUATION MODULES:
/cfs-file/__key/communityserver-discussions-components-files/158/swru410a.pdf…