Hello all, We have purchased an evaluation board of OPA862D. The default configuration of module during shipment is 4V/V. In the termination network, their is attenuation of -38 dB, this results in the overall gain to be -26 dB. The input and output signals is single ended. This is the default configuration of module.
I want the module to give a gain of 1V/V, i.e., for 2V input (single ended), the output should be 2V (Differential).
I request, if anyone can provide me the procedure of reconfiguring OPA862DEVM module to achieve the task. Thank you in advance.
The datasheet is attached.