This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA200-Q1: Typical application parameters in Table 1

Part Number: INA200-Q1
Other Parts Discussed in Thread: INA200

Hello Support team,

I can find the below typical application in the datasheet.

According to Table 1, 

VOUT_TRIP = ITRIP x RSHUNT x Gain = 1A x 5mΩ x 20V/V = 0.1V

R2 / (R1+R2) x VOUT_TRIP = 15 / (10+15) x 0.1V = 0.06V

Therefore, I guess that Table 1 design can't work at ITRIP=1A.

Is it wrong description in the datasheet?

Best Regards,

Hirokazu Takahashi