Part Number: PGA309
Other Parts Discussed in Thread: MULTI-CAL-SYSTEM,
To whom it may concern,
I initially tried to use the supplied RS-232 cable to communicate to the HP34401A VOM with the Multi Cal system. After setting up the multimeter I could not communicate with the VOM. Luis at TI suggested that most use the Multi Cal system with the GPIB interface. I have configured the VOM to communicate via the GPIB interface and assigned it the address "2". I have also assigned the script "2" as well. The program insists the address is invalid. I have verified the USB to GPIB converter is seeing the VOM (See attached word doc.) The address the program is using is identical to the address recognized by the converter program (See again word doc attached). I have attached the script I'm using as well. Any help is welcome.
Best,
Joe
IEEE488_address> 2 pause> 2.0 write> MEAS:VOLT:DC? 10,0.00001 read_dbl> 64