Other Parts Discussed in Thread: TINA-TI, OPA2990, RC4560, RC4580, LM833, NE5532, OPA1678, MC33078, LM358, NE5534
It probably isn't going to thrill anyone here to hear that I'm doing my SPICE analysis with LTSpice not TINA-TI, but I already have an active (and still unanswered!) issue with DesignSoft about issues having to do with transformer models that LTSpice was already intrinsically compatible with, but you need to understand that I'm in the final design phases of my next product design, and any part that I can't get a "clean" simulation for is a part that I'm not going to submit a volume purchase order for, so please see to it that I get the support I need! So I'm trying to simulate this circuit using op amps in a certain range of slew rate, voltage compatibility and output drive, and there just aren't a large number of parts meeting those criteria, so I'd like to try and find models for as many of these part numbers as possible. So I haven't yet found any parts that exactly meet my criteria, but here is a list of the parts I was having issues with, I would like to know if you have any answers for these issues:
OPA2990 - no model file (apparently there used to be a sboman9.zip but it's no longer available)
RC4560 - no model file found
RC4580 - unbelievably the only file available is a sloj175.zip which is in ENCRYPTED HSPICE, and no means of DEcryption appears to be provided
LM833 - there's a file snlm202.zip but it doesn't work correctly. This one is really interesting, LTSpice keeps emitting this error "Def Con 1!" and throwing up all over the place, actually here's a partial copy of the error log:
Circuit: * C:\Users\New\Documents\LTspiceXVII\out833.asc
ERROR: Node U1:I0:I21:1:102 is floating and connected to current source G:U1:I0:I21:1:RA
ERROR: Node U1:I0:I19:1:102 is floating and connected to current source G:U1:I0:I19:1:RA
ERROR: Node U1:I0:I19:1:302 is floating and connected to current source G:U1:I0:I19:1:RC
ERROR: Node U2:I0:I21:1:102 is floating and connected to current source G:U2:I0:I21:1:RA
ERROR: Node U2:I0:I19:1:102 is floating and connected to current source G:U2:I0:I19:1:RA
ERROR: Node U2:I0:I19:1:302 is floating and connected to current source G:U2:I0:I19:1:RC
ERROR: Node U3:I0:I21:1:102 is floating and connected to current source G:U3:I0:I21:1:RA
ERROR: Node U3:I0:I19:1:102 is floating and connected to current source G:U3:I0:I19:1:RA
ERROR: Node U3:I0:I19:1:302 is floating and connected to current source G:U3:I0:I19:1:RC
u3:vpd: Missing value, assumed 0V @ DC
u3:i0:vprobe2: Missing value, assumed 0V @ DC
u3:i0:vprobe1: Missing value, assumed 0V @ DC
u2:vpd: Missing value, assumed 0V @ DC
u2:i0:vprobe2: Missing value, assumed 0V @ DC
u2:i0:vprobe1: Missing value, assumed 0V @ DC
u1:vpd: Missing value, assumed 0V @ DC
u1:i0:vprobe2: Missing value, assumed 0V @ DC
u1:i0:vprobe1: Missing value, assumed 0V @ DC
Direct Newton iteration failed to find .op point. (Use ".option noopiter" to skip.)
Starting Gmin stepping
Gmin = 10
Gmin = 1.07374
vernier = 0.5
vernier = 0.25
vernier = 0.125
vernier = 0.0625
Gmin = 0.687195
vernier = 0.03125
vernier = 0.015625
vernier = 0.0078125
Gmin = 0.668762
vernier = 0.00390625
vernier = 0.00195313
vernier = 0.000976563
vernier = 0.000488281
Gmin = 0.669252
Gmin = 0
Gmin stepping succeeded in finding the operating point.
Heightened Def Con from 1.95313e-009 to 1.95703e-009
Heightened Def Con from 1.95703e-009 +to 1.95898e-009
Heightened Def Con from 1.96387e-009 to 1.96411e-009
Heightened Def Con from 1.9646e-009 to 1.98022e-009
Heightened Def Con from 2.06274e-009 +to 2.18774e-009
Heightened Def Con from 2.40649e-009 to 3.40649e-009........
Can you help me actually resolve any of these issues and find a part that gives me a "clean" simulation? (I'm NOT at liberty to provide the actual schematic as it's LOADED with proprietary IP!) Thank you!