Part Number: TLV3702
Other Parts Discussed in Thread: OPA657
Hello,
we wan't to model our signal chain as accurate as possible. Can you share the input capactitance of the TLV3702 and OPA657?
Thank you and best regards,
Ambroise
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ambroise,
Thank you for your question. Typically, the input capacitance of the TLV3702 is less than 10 pF.
Since I am assuming this is not a fast application, I would recommend placing a 100 Ω or 1 kΩ resistor between the output of the op amp and the input of the TLV3702 if the OPA657 is driving the inputs of the comparator.
Are you driving an input of the TLV3702 with the output of the OPA657?
Best Regards,
Joe
Applications Engineer
Linear Amplifiers Business Unit | Comparators Product Line (CMPS)
All information in this correspondence and in any related correspondence is provided “as is” and “with all faults”, and is subject to TI’s Important Notice (http://www.ti.com/corp/docs/legal/important-notice.shtml)