Part Number: VFC320
Other Parts Discussed in Thread: TINA-TI,
Hi,
My question is regarding the frequency to voltage conversion application, with frequency in the 10KHz range and output voltage of 1V full-scale.
The datasheet indicates the comparator at pin10 will register logic "0" at 0V or below, and logic "1" at 1V or above.
The waveform in figure 9 shows crossing of 0V followed by 1V at the falling edge of the input signal.
In my design, because of small signal swing (1.8v), the logic "0" and logic"1" are crossed at the opposite edges of the input wave. Logic "0" is registered at the falling edge, and logic "1" is registered at the rising edge.
Will this be a problem to the one-shot circuit?
And, is there a model I can input to TINA-Ti to simulate?
Thanks