Hi Team,
My customer is using AMC1200 to monitor the voltage of battery pack (400V). About the input anti-aliasing RC filter, we found some interesting things as bellow:
1) Figure A, with RC filter (10ohm, 330pF), the sampling result is accurate, ±2V variance.
2) Figure A, without RC filter (10ohm, 330pF), the sampling result is accurate, ±2V variance.
3) Figure B, short 2 Resistor, with only C filter (330pF), the sampling result has -20V to -5V bias, bellow is the sampling results.
Could you help comment why the result will have bias if only has C filter (I have run the simulation and found that the frequency response of case 2) & 3) are the same)?
|
|
Result |
VOUTP |
VOUTN |
VOUTP - VOUTN |
Test 1 |
AMC1200 Sampling |
338V |
3.162V |
2.039V |
1.123V |
Actual Value |
350V |
3.13V |
1.97V |
1.16V |
|
|
|
|
|
|
|
Test 2 |
AMC1200 Sampling |
188V |
2.91V |
2.288V |
0.622V |
Actual Value |
200V |
2.8814V |
2.2186V |
0.6628V |
Thanks a lot.
Best regards,
Yang