Part Number: LMV762
Hi Team,
The customer is using LMV762Q-Q1 dual package comparator in their project but they are not using one comparator section and they are asking what is the best way to terminate that unused comparator's input & output pins.
What I recommend was to follow the advice on this thread however, they have very limited space on their board, and following the advice on the thread would not be possible. Could you share the reason for connecting midsupply to one input? Is it necessary to connect one input to IC supply with divider network?
Can you also confirm if following the "Application Design Guidelines for LM339, LM393, TL331 Family Comparators (Rev. B)" Sec 5.1 Unused Comparator Connections would be okay? kindly refer to the image below:

Thank you for the support.
Regards,
Marvin