Other Parts Discussed in Thread: OPA2333P, INA185, MC33078, OPA2333
Hi There,
I am using LMV358 in differential amplifier configuration with a gain of 50 to measure current using shunt resistor. The value of shunt resistor is 250uohm (8 x 2mohm resistors in parallel). Please find attach schematic for your kind reference. Please note that we have used both opams for bi-directional current measurement with inputs of second OPAM inverted.
Issue : In standby condition, we are observing the output of 100mV. The voltage across BAT-_P and BAT-_N is 0V but voltage across pins 2 and 3 is 2.3mV. This 2.3mV with a gain of 50 is giving output of 100mV in standby condition. Due to this we are unable to measure current less than 8A. Request you to provide your inputs to remove this offset of 100mV somehow.
Note : We isolated inputs to 2nd opam and measure the output and it still remains 100mV for the 1st opam output, so 2nd opam with inputs is not creating any issues.
Thanks..!!!