This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA552: Output Resistance of OPA552

Part Number: OPA552
Other Parts Discussed in Thread: OPA551,

I want to know the output resistance (Ro) of this OpAmp

  • Hello Preetham,

    I searched our archives for OPA552 Zo and didn't find it for that op amp. I did find the Zo curve for the OPA551 which is the unity gain stable version of the same amplifier. The OPA552 Zo will be the same at lower frequencies, but I expect it will deviate somewhat at higher frequencies because it is a decompensated version having higher bandwidth than the OPA551.

    The OPA552 is a legacy op amp and it has an older simulation model design. I checked the model and it models Zo as a constant 25 Ohms across frequency.

    This is the extent of Zo information we are able to provide for the OPA552.

    Regards, Thomas

    Precision Amplifiers Applications Engineering