Part Number: OPA549
Other Parts Discussed in Thread: OPA593, , OPA541
Dear Team,
I want to make single supply power amplifier. The given conditions are as follows.
1. Input Signal : From AD5932 (Programmable Frequency Scan Waveform Generator)
- Peak to Peak : 0.58V (Internal 200ohm resistor to GND)
- Voltage at midscale output : 0.32V
- Minimum Voltage : 56mV
2. Wanted Output Voltage : 0 ~ 24V ( If it is not possible, please let me know the allowable range.)
3. Wanted Output Frequency :250KHz ( If it is not possible, please let me know the allowable range. )
Please recommend a circuit that can be implemented.
Sincerely,
Eui-heon