This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA549: Single Supply Power Amplifier

Part Number: OPA549
Other Parts Discussed in Thread: OPA593, , OPA541

Dear Team,

I want to make single supply power amplifier.  The given conditions are as follows.

1. Input Signal : From AD5932 (Programmable Frequency Scan Waveform Generator)

    - Peak to Peak : 0.58V (Internal 200ohm resistor to GND)

    - Voltage at midscale output : 0.32V

    - Minimum Voltage : 56mV

2. Wanted Output Voltage  : 0 ~ 24V ( If it is not possible, please let me know the allowable range.)

3. Wanted Output Frequency :250KHz ( If it is not possible, please let me know the allowable range. )

Please recommend a circuit that can be implemented.

Sincerely,

Eui-heon