As stated above have a application for an OEM that needs around a100w at 1 ohm while running off of 14.4v DC no boost supply.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As stated above have a application for an OEM that needs around a100w at 1 ohm while running off of 14.4v DC no boost supply.
Hey Joe,
14 amps is much more than any general purpose amplifier can supply. Would they be open to a topology of an op amp driving a FET? Then they could drive an external FET that can provide much more output current than the amplifier can.
Best,
Jerry
There is actually a ST that we are using now that basically does this its 92w at 1 ohm 10% thd we are looking to replace this chip with a TI option if possible if not we will build a discrete one
Hey Joe,
We do have a selection of power amplifiers. I will move this thread to the precision amplifiers team and they would be happy to assist you!
Best,
Jerry
Hi Joe,
As stated above have a application for an OEM that needs around a100w at 1 ohm while running off of 14.4v DC no boost supply
Can you specify if the power application is DC or AC? If it is AC application, please specify the op amp's operating frequency, voltage amplitude and current etc..I'd like to know the design requirements.
I assumed that you are talking about 1ohm load with the wattage of approx. 100W, which is the circuit output voltage at approx. 10V in DC (V*V/R = 100W at the load).
Best,
Raymond
Hi Joe,
please specify the op amp's operating frequency, voltage amplitude and current etc..I'd like to know the design requirements.
If this is DC application with supply rail of 14.4Vdc, where op amp's Vout = 10V, 1Ω load @10A, then it is much simpler. We just need to make sure that heat dissipation across the power amplifier will be low.
You may need to reduce the supply voltage from 14.4Vdc to 12Vdc or so, then the heat dissipation at driving power amplifier will be reduced significantly, and it is likely that PRAMPS may accommodate for that.
Best,
Raymond
Hi Joe,
Our OPA541 is able to source 10Adc continuously, but the input and output driving application have certain constraints.
If this is DC power application or you will use the power amplifier as a voltage regulator to drive 1Ω at 10Adc, I would recommend to build a low drop out series voltage regulator. We have many highly accurate LDO that will meet your need at the current level.
If this is for AC application, I need to know the application requirements.
Best,
Raymond