The existing spice model in TI database, doesn't support monte-carlo variations, would it be possible to support by providing a revised model which can support MC variations ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The existing spice model in TI database, doesn't support monte-carlo variations, would it be possible to support by providing a revised model which can support MC variations ?
Hi Xinchao,
My colleague did make a sub-circuit that would allow an amplifier model to run a Monte-Carlo simulation of input offset voltage, but I haven't used it yet for any amplifier models. I don't know of any model that also includes standard deviation information for parameters in addition to input offset voltage.
Although we usually treat the datasheet's typical input offset voltage as a DC value in the model, in reality this value is 1 standard deviation, and the bell curve is truncated at the max and min values. For a monte carlo analysis, the offset distribution of offset voltages should be centered around 0V.
You can use a DC voltage source to cancel out the model's internal input referred offset voltage, and then use a second input DC voltage to act as the offset voltage with the standard deviation specified.
Best regards,
Sean