This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903V: What devices corresponding to Red-Bull for LM2903VQDRQ1

Part Number: LM2903V
Other Parts Discussed in Thread: LM2903B, LM2903,

Hi good day,

 

This is Enzzo from Taiwan CM4. Automotive is an important area that we want to grow faster. EV head lights are one of the most important EE in Automotive.

Recently our customer USI have a project for headlight turn indicator. The run rate is 160 K/year (80K vehicles). To avoid shortage problems. Have a question for LM2903VQDRQ1.

If LM2903VQDRQ1 have any device corresponding to Red-Bull device? (if pin2pin or not)

Thank you.

 

 

Warm wishes,

 

Enzzo Fan

Technical Sales Associate

  • Enzzo

    Thank you for reaching out.  Can you obtain a schematic or additional details regarding their system requirements of the comparator?  From this information, we should be able to provide alternative solutions.  However, in the case of LM2903, we have already released our new version called the LM2903B.  the automotive orderable for the SOIC option is 

    LM2903BQDRQ1

    Chuck

  • Hi This is the information for this project.

    Can you provide the comparison table of LM2903VQDRQ1?

    Thank you.

  • Enzo

    thanks for sharing the additional information.  unfortunately, I cannot read the schematic which would provide the information needed to select alternative options.  I am going to close this post and connect you with our team offline that supports the LM2903 family.  For starters, you can find a simple comparison table of the original LM2903V and our LM2903B at the bottom of the front page of the datasheet.

    Chuck