Part Number: LM2904B
Other Parts Discussed in Thread: UCC28951, LM2904,
Hi,
My customer is facing a problem when use LM2904B to replace LM2904AV, as showed in the schematic below, customer is using LM2904 for a current and voltage sampling for a PSFB with using UCC28951.
When using LM2904B, they found that the Vadj is turned down when the input voltage is high, namely the current in COMP of UCC28951 is high. However, with LM2904A it doesn't occur.
Also, when customer changed the R406 and R431 in second figure from 100kohm to 50kohm, the Vadj value turned up a little bit. The normal voltage on Vadj is around 2V.
Customer would like to know, what differences between LM2904A and LM2904B that may cause that only LM2904B have this problem?


Thanks!
Manu