This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH32404-Q1: LMH32404

Part Number: LMH32404-Q1

Hello,

I want to drive the VOCM pin to 0.7V.

How I override the 1.1V internal bias?

                                           How to drive?

Regards,

Giora

  • You device must be strong enough to override the internal resistor divider. The VOCM input impedance is specified as about 17 kΩ. If you are using an opamp, it will usually be much stronger than that.

    In theory, you could use a plain pull-down resistor of 29.68 kΩ, but in practice, I do not know the tolerances of the internal resistors.