Part Number: OPA549
Hi Team,
I am making a voltage controlled voltage source with OPA549, the following is the schematic diagram, I encountered two problems during use:

1) The power-on sequence of VIN+ and VIN- seems to have requirements: under no-load condition, the Ctrl terminal is always shorted to SGND. If VIN+ is powered on first, before VIN- is powered on, VOUT will output a voltage close to VIN+ ; Similarly, if VIN- is powered off first, VOUT will output a voltage close to VIN+. As shown below

Black: VIN+; Blue: VOUT; Rose: VIN-
But that voltage is pulled down to zero by a certain amount of resistance (in the order of hundreds of ohms). Why does the power-on and power-on sequence affect the output? This is not reflected in the D/S.
2) There will be some ringing and stable low frequency oscillation when the output is connected to no-load or capacitive load. These oscillations will also be damped by a certain amount of resistive load, but is there any other better method?

Blue: Ctrl; Black: VOUT; Green: IOUT
-A