This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA213: EE product info

Part Number: INA213

Team,

Customer is setting up INA213CIDCKR in system and would need to know these parameters that seems not stated in datasheet. Can you help to check and advise? Thanks.

(EE)_* Preheat/Soak Time between 150~200℃ (s) MAX:

 

(EE)_* Preheat/Soak Time between 150~200℃ (s) min:

 

(EE)_* Ramp-up rate (℃/s):

 

(EE)_* Liquidous temperature Time maintained above 217℃ (s) MAX:

 

(EE)_* Liquidous temperature Time maintained above 217℃ (s) min:

 

(EE)_* Peak package body temperature (℃):

 

(EE)_* Time* within 5℃ of the specified classification temperature (s):

 

(EE)_* Ramp-down rate (℃/s):

 

(EE)_* Time 25℃ to peak temperature (s):

 

 

 

* Power Dissipation(Pd) (W):

 

* Rated Voltage (V):

 

*Rated Current (A):